STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 Wakeup from UART in stop mode 1

Hi all,I've been struggling so much to get wake from uart working on this board. It looks like it should be simple, I have this code which I am pretty sure should be everything needed, but it just doesn't wake up when I send data to the serial port.C...

Alan01252 by Associate II
  • 309 Views
  • 19 replies
  • 2 kudos

Resolved! STM32U5 File system with FreeRTOS

Hello,I'm using NucleoU575 with CubeMx and I want to make a file system on my SD card.I want to use FreeRtos but there are no Fatfs in CubeMx and the FileX cannot work with FreeRtos (image). Is there anyway i can use Fatfs with STM32U5 ?Thank you. 

_legacyfs_online_stmicro_images_0693W00000bk2bEQAQ.png
M326.1 by Associate II
  • 5414 Views
  • 6 replies
  • 1 kudos

Encrypted DFU Custom Bootloader

Hello,What is the simplest and best way to implement encrypted firmware update via DFU?  I plan on building a custom bootloader but have not found any recent existing projects.  I tried STM32-AES-Bootloader but it is setup for STM32F10 and I am using...

LMorr.3 by Senior II
  • 177 Views
  • 1 replies
  • 0 kudos

NUCLEO-N657X0-Q Flash partition FileX

I have a project working on the NUCLEO-N657X0-Q with FSBL and an application. In total I am using under 1MB of the 64MB flash this board has. I was wondering if it was possible to segment off the rest of the flash to be used as a mass storage device ...

neil1106 by Associate II
  • 121 Views
  • 0 replies
  • 0 kudos