STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL L4 RTC Bug Report

I'm currently using a STM32L433RCT3 and the L4 HAL library. My goal was to read back a configured RTC alarm, increment it, and restart the alarm. I created a:RTC_AlarmTypeDef sAlarm;I read back the RTC alarm using,HAL_RTC_GetAlarm(&hrtc,&sAlarm,RTC_A...

MVeen.1 by Associate II
  • 1737 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 USBX hub class flaky - Bug???

There seems to be a bug when using the USBX hub class.  Sometimes it works, but most often it does not.  The problem appears to be with file: ux_host_stack_enum_thread_entry.c.  The code:  VOID _ux_host_stack_enum_thread_entry(ULONG input) { UX...

matt-crc by Senior III
  • 1792 Views
  • 7 replies
  • 3 kudos

STM32F103RBT6 USB problem

Hello, I have a problem with communication between my PC and MCU. I have connected my project according to this diagram (with external 12MHz oscillator):  I attempted to connecting the 1,5k GPIO pin (PA10) to control the pull up. Then I connected a 1...

radekklepal99_0-1741793253915.png radekklepal99_0-1741794688405.png radekklepal99_1-1741794719699.png prtscr1.jpg

Resolved! HAL_I2C_Mem_Read disables interrupts

I have set up a STM32F103 as a I2C master. I have found that calling the function HAL_I2C_Mem_Read sometimes disables all interrupts for more than 140us. Needless to say this causes significant problems with the timing of other external interrupts. T...

JGaby.1 by Associate III
  • 2211 Views
  • 5 replies
  • 1 kudos

How to connect a removable sim (not truphone) with B-L462E-CELL1? Some AT commands don't work neither in X-Cube-Cellular nor by talking with the modem directly through USART3.

I've been trying to connect the modem for weeks (Not the truphone sim, a removable one). I would like to connect by talking with the modem directly (through the AT commands), however I have also tried the X-Cube-Cellular.Some AT commands don't work n...

0693W00000GVtWNQA1.png
SPere.2 by Associate III
  • 1873 Views
  • 3 replies
  • 0 kudos

HAL_DSI_Init() stuck on error

Hi,the application gets stuck on the Error_Handler() in the piece of code below in main.c    hdsi.Instance = DSI; hdsi.Init.AutomaticClockLaneControl = DSI_AUTO_CLK_LANE_CTRL_DISABLE; hdsi.Init.TXEscapeCkdiv = 4; hdsi.Init.NumberOfLanes = DSI_...

Ricko_1-1741496086965.png Ricko_2-1741496396470.png Ricko_0-1741496058160.png
Ricko by Senior III
  • 1216 Views
  • 1 replies
  • 0 kudos