STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I configure/program with MDMA?

Hi All,I am struggling with that the maximum DMA buffer size is 64KB. I am currently transferring the data from an ADC to the Buffer using DMA with circular buffering, but I would want the buffer to be around 200KB. I have heard that one can use MDMA...

elso by Senior
  • 4932 Views
  • 6 replies
  • 0 kudos

Query regarding USBH_HID_GetReport

Hi I am trying to read a report of USB HID device from my STM32 USB Host code.I am able to read the report descriptor successfully from USBH_HID_GetHIDReportDescriptor call.I wanted to read the 0xD0 report value using if(USBH_HID_GetReport (phost,   ...

PSaba by Associate
  • 1632 Views
  • 1 replies
  • 0 kudos

[Synopsys OTG] FIFO clash

So where exactly does the documentation say that different FIFOs can't be accessed simultaneously?In dervice mode, an In endpoint was configured to transmit one 16-byte-long packet, and then 16 bytes (i.e. 4 words, 72 43 70 A4 D9 99 55 2E 19 7F 32 37...

0690X000006C5xoQAC.png

Resolved! No Example QSPI SDK for STM32F413H

Hi i am using Nucleo - F413ZH i need to work on the QSPI protocol i found this device supports QSPI but in the repository i doesn't find any example code for this one is this device supports QSPI? or is there any similar sdk so that we can import pro...

avinpat_8_0-1742817721795.png
avinpat_8 by Associate III
  • 2163 Views
  • 6 replies
  • 0 kudos