STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H750 UART latency [Zephyr]

I am using an STM32H750 custom hardware to interface with an external UART device at 38400 baud. (see STM32_block.png). UART 2 is configured to Asynchronous mode.It is used to transfer the following 31 bytes of data to the external deviceff 03 fe f0 ...

High output frequency from DAC

Split from https://community.st.com/t5/stm32cubeide-mcus/problem-with-file-ioc-quot-not-a-valid-ioc-file-quot/td-p/791325 as this is a new questionBut now, I have another question. The file I use is one of the example on stm32G431RB "DAC_SignalGenera...

mala by Associate II
  • 2027 Views
  • 4 replies
  • 2 kudos

Resolved! TIM encoder mode with Encoder clock output

I try to combine the enocer mode of TIM1 with a encoder clock period measument using TIM8. The RM0456 (for U5) mentions this in the end of chapter 54.3.25 under the heading "Encoder clock output". TIM1 works fine and counts up and down according to t...

stryga by Associate III
  • 1306 Views
  • 1 replies
  • 0 kudos

Resolved! STM32N6 getting stuck in USB_CoreReset( )

I urgently need to get USB High Speed working on USB1 of the STM32N6570-DK. I have attached the .ioc file I am using.I am able to get the GPIO_IOToggle project working on the board. I am able to put breakpoints step through the code.I am using  STM32...

STM32F100C8T6B Bootloader issues

Posted on December 03, 2012 at 20:42I am trying to talk to the bootloader in the STM32F100 and having some issues. I can successfully send the 0x7F and get back a 0x79 ACK. Next when i send a Get Command i don't get any response. I am sending two by...

Resolved! Nucleo-U031R8 UART examples do not work?

Hi to all.I'm testing the Nucleo U031R8. To avoid the Package issue i switch also to the old package firmware version (1.0.0), but same error.The example is UART_HyperTerminal_IT  and i simple cloned (or compiled directly in the repository), then exe...

TheRaprus by Associate III
  • 2200 Views
  • 4 replies
  • 1 kudos