STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FREERTOS: Binary-Semaphore initial state bug

Hello Experts,i am facing a similar issue on the STM32F407G discovery board. Is there any solution or a temporary fix for this iisue?https://community.st.com/t5/stm32cubemx-mcus/re-freertos-semaphore-not-initialised-correctly-by-cubemx/td-p/780252 Ch...

ak52_1-1747402483298.png ak52_2-1747402578968.png ak52_4-1747403494153.png ak52_3-1747403159242.png
ak52 by Associate III
  • 3988 Views
  • 4 replies
  • 1 kudos

Resolved! Why does CORDIC give not accurate results?

Hi all.I have this piece of code: __HAL_RCC_CORDIC_CLK_ENABLE(); CORDIC->CSR |= CORDIC_CSR_NARGS; CORDIC->CSR |= (CORDIC_CSR_PRECISION_3 | CORDIC_CSR_PRECISION_2 | CORDIC_CSR_PRECISION_1 | CORDIC_CSR_PRECISION_0); CORDIC->CSR |= CORDIC_CSR_FUNC_1...

yonatan by Associate III
  • 1682 Views
  • 3 replies
  • 0 kudos

Record audio using PDM OR DFSDM

Hi, I am working with STM32H757I-EVAL. The task is to record audio, store it in SD Card. Since, STM32H757I-EVAL has PDM Data format as well as DFSDM data format which would be better to interface with or is there anyother data format that can be used...

priya_12 by Associate II
  • 1044 Views
  • 1 replies
  • 0 kudos

Moving code from G030 to C011

Hi All I have a breakout board, I've been testing some ws2812 code , I'm using  TIM1 with DMA + PWM I developed the code on the G030, it's a 32 pin package. I'm using internal clock and have it running at 48MHz for Timers. Works has intended.    Swit...

stevecimo by Associate III
  • 5147 Views
  • 19 replies
  • 2 kudos

Measuring problem

Hello,  I have a problem with my code, I have a 1PPS signal from a GPS on a PB0 input, I want to measure a 10.00Mhz signal on the PC0 input. I have a uart4 tio display the result. My problem is that the result is always zero on my screen "Frequency 0...

PSEBA.1 by Associate II
  • 863 Views
  • 0 replies
  • 0 kudos