STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5A9 and X-CUBE-AUDIO?

Hi,I'm getting info on playing mp3 files with my custom Nucleo-U5A9 (originally a NUcleo-U575, I replaced the MCU and added xtal). I'll be using the audio codec TLV320AIC3110 with I2C and SAI from the U5A9. I'll be using ThreadX, FileX an a uSD card....

Rodo by Senior
  • 511 Views
  • 4 replies
  • 1 kudos

STM32H735G-DK can't change pixel format mode

Hello,I'm working on the STM32H735G-DK and try to change LTDC pixel format mode on the fly, but it doesn't work. I'm using the BSP example from example board pack in CubeMX for this board. After reset is possible setup the first time pixel format, bu...

wegi01 by Associate III
  • 191 Views
  • 2 replies
  • 0 kudos

Resolved! Use external NOR flash to move CPP object file

Hello,I have STM32F7 controller, using Free RTOS, trying to interface external NOR flash, S29GL128S10TFIV13.I have one source file say testCode.cpp, which I want to move completely in external NOR flash, but every time I ran then code it give Hardfau...

Resolved! ADC Sampling and Display

As is well known, the ADC sampling rate is on the order of microseconds, while the display task may only refresh once every 100 milliseconds. In an RTOS, how can the display task and ADC sampling values be synchronized? With such a long display refre...

xwq370 by Associate
  • 161 Views
  • 2 replies
  • 0 kudos

Resolved! X-CUBE-GNSS1

I have a project that will be using the LIV4F chip. I downloaded and installed X-CUBE-GNSS1 but its description says it is for the LIV3F. Is it compatible with and will it function with the LIV4F chip? I will be using it on the STM32G474CEU6.Thanks!

hritter by Associate II
  • 126 Views
  • 1 replies
  • 0 kudos