STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32N6 VENC Power measurement example code

Good day folks!I trust you are well.Do you know where I can find the example that was used to take the VENC power measurements as outlined on this Wiki page ?I can't seem to find it under the Applications and Examples in the STM32CubeN6 v1.2.0 Specif...

exarian_0-1752838699556.png
exarian by Associate III
  • 598 Views
  • 2 replies
  • 0 kudos

Resolved! SPI in STM32F427 in slave mode

Hi, gents,     I have some need to use SPI slave mode instead of working SPI master mode.     I'm tranferring 22 16-bit words from Infineon slave board at 6Mhz clock rate, once per 100 ns, and have 4-line interface including CS line. Due to noisy lin...

DR77 by Associate II
  • 1447 Views
  • 3 replies
  • 0 kudos

STM32N6 VENC at lower resolutions

Hi everyone,I have successfully deployed the VENC_SDCARD example on the board and can see its feed on my laptop. Now, I want to record it at 480x480 resolution instead of the default 800x480 provided in the example.I have modified the buffer size, DC...

Image (1).jpeg Screenshot from 2025-07-15 13-41-14.png

Clock / Timing problem in I2C

I am trying to run a loopback test with 2 i2c's on the same board. The onboard leds need to light up on successful transmission and reception, the problem is the leds light up when in debug mode, going line by line, but not in stand#define I2C1_ADD (...

maya16 by Associate III
  • 626 Views
  • 3 replies
  • 1 kudos