STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Porting of HID USB on FreeRTOS

Posted on January 26, 2012 at 19:27Hi I am having issue of porting USB to FreeRTOS environment, Windows pops up and message in task bar saying ''Unknown Device ''   Please help., Does it mean USB it set at wrong clock, USB used to be so simple on ST...

STM32F4xx - Ethernet MII/SMI clock (

Posted on October 04, 2012 at 14:26For setting of the divider, which determines the Ethernet MAC-to-PHY Serial Management Interface's (MDC/MDIO lines) clock rate, the stm32f4xx.h header says the following:&sharpdefine ETH_MACMIIAR_CR   ((uint32_t)0x...

USB CDC Serial Port

Posted on June 10, 2011 at 21:14Hi, I am concepting a new design that has to communicate using USB.  I have a pivitol question.  Is it possible to implement a USB interface that emulates a PC COM port that will install under Windows without having a...

longTimer by Associate II
  • 4511 Views
  • 8 replies
  • 0 kudos

FATfs Writing Data to Created Files Issue

Posted on July 31, 2012 at 15:05Greetings, I have been working with implementing FATfs for reading and writing to a microSD card. This is being done on an STM32L discovery board in the IAR Embedded Workbench environment. The issue that I am having i...

evans by Associate
  • 2564 Views
  • 4 replies
  • 0 kudos

Ethernet reference design

Posted on September 10, 2012 at 10:26Hello, some time ago I opened a ticket for a techincal support about this topic but I never received an asnwer. So I try to ask here. The schematic of STM32F207ZG-SK_Rev.C use an STE101P for the Ethernet interfac...

Mark81 by Associate III
  • 2881 Views
  • 2 replies
  • 0 kudos

Virtual COM and GPIO_Pin_10 from GPIOA

Posted on May 24, 2012 at 13:07 Dear all, We have recently developed a board that includes the STM32F103CB microcontroller (36-pin version) and has a USB connection (mini-USB) to power the device and also to communicate with a computer. ...

peretuset by Associate II
  • 2205 Views
  • 6 replies
  • 0 kudos

Restart ISP bootloader from application?

Posted on August 31, 2012 at 10:55Hello, is there any way to restart the built-in ISP bootloader from the application? Any particular start address to jump to? If the boot loader is located at the start of the system memory, would it work to simply ...

tilmann by Associate III
  • 1275 Views
  • 2 replies
  • 0 kudos

stm32f4 discovery board USB Driver

Posted on August 28, 2012 at 23:18I have got a f4 discovery board and a device with USB interface, I want to send the Command to this device and receive the data from it, but I do not know how can I do it. Can I use the USB-OTG-Host example? Who can...