cancel
Showing results for 
Search instead for 
Did you mean: 

Restart ISP bootloader from application?

tilmann
Associate III
Posted on August 31, 2012 at 10:55

Hello,

is there any way to restart the built-in ISP bootloader from the application? Any particular start address to jump to? If the boot loader is located at the start of the system memory, would it work to simply jump to 0x1FFFF000 (+1 for thumb)?

(Devices currently are differently sized F103 types, but I think this is a general question...)

Thanks, Tilmann

#isp-bootloader-restart
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 31, 2012 at 13:28

0x1FFFF000 contains a stack pointer

The problem with just calling the address stored at 0x1FFFF004 is that you probably aren't running the processor at ''reset'' conditions, figure interrupts, pll, clocks, etc.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32 Internal Bootloader&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=2980]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2FSTM32%20Internal%20Bootloader&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=2980

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
tilmann
Associate III
Posted on August 31, 2012 at 14:59

Clive,

many thanks for your fast answer!

If it's not documented what the bootloader really does (or expects) during initialization, it really sounds reasonable to use the system reset... Thanks for the link to the other post (which I interestingly didn't find using the forum search...).

Have a nice weekend,

Tilmann