STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f2 FIFO_FS_SIZE

Posted on April 22, 2013 at 10:14I am use stm32f207vc usb FS devices mode. The IN_EP = 0x82 ;  OUT_EP = 0x03; the EP1 is no use. and I want to know how to setting the FIFO_FS_SIZE?? the VCP demo is: &sharpifdef USB_OTG_FS_CORE  &sharpdefine RX_FIFO_...

easylwl by Associate II
  • 1776 Views
  • 3 replies
  • 0 kudos

ST Boot support download with offset

Posted on April 10, 2013 at 16:25Does the Boot loader of ST (DFU) support download FW for diffrent location then start of FLASH? What I mean is can I use it to burn my BOOT IAP application first on 0x08000000 with Boot hex file and then go again and...

Barbie by Associate II
  • 891 Views
  • 1 replies
  • 0 kudos

uIP question

Posted on December 24, 2012 at 17:41 uint32_t uIPMain( void ) { uint32_t i; uip_ipaddr_t ipaddr; struct timer periodic_timer, arp_timer; // Sys timer init 1/100 sec tick clock_init(2); timer_set(&periodic_timer, CLOCK_SECOND / 2); timer_s...

STM32F4DIS-EXT - UDP

Posted on April 08, 2013 at 03:29Hi Guyz, I would like to send a udp data using the STM32F4DIS-EXT board / STM32f4DIS-BB (serial/LAN/SD). Can someone guide me how... ( I am now browsing the examples) #lwip #lwip #ip #ip #udp #udp

xtian by Associate II
  • 2263 Views
  • 5 replies
  • 0 kudos

STM32F107 + DP83848(Ethernet controller)

Posted on September 01, 2011 at 10:37Hello, I have a problem with the ethernet controller DP83848 in combiantion with a STM32F107.  I designed a PCB with these two components, I copied a part of the schematic of the STM3210C-EVAL board. I am using t...

Porting from STM32F4 to STM32F1

Posted on April 04, 2013 at 14:52Hi, I have a big problem. I'm trying to port an application I found for STM32F4 mcu to a STM32F107VC mcu. This application uses lwip for ethernet and FreeRTOS. I try a lot but cannot compile an application that runs....

tommaso by Associate II
  • 1280 Views
  • 2 replies
  • 0 kudos

Low power USB host solution

Posted on March 30, 2013 at 12:43Hi all, I'm using STM32F100 processors for a while now and i had no issue so far. I'm looking for a solution that provides USB host functionality to a Flash disk but it must  be powered by battery, so it must by ener...

BootLoader with AN2557 creat bin file

Posted on March 25, 2013 at 16:10For the demo example AN2557 1.does it need a special bin file to creat, because standard bin file doesn't contain the format show in the YMODEM.c ? 2.Does this format made by the UART modem if put in YMODEM? 3.What ...

Barbie by Associate II
  • 946 Views
  • 1 replies
  • 0 kudos

STM32F4discovery high speed USB

Posted on December 26, 2012 at 05:46hi     how can I get high speed USB interface to host a device on STM32F4discovery?     would i have to remove component from the kit OR just add additional PHY? #high-speed-usb #usb-otg #cpen #otg_hs #highspee...

its by Associate II
  • 6537 Views
  • 16 replies
  • 0 kudos