2012-12-24 8:41 AM
uint32_t uIPMain(
void
)
{
uint32_t i;
uip_ipaddr_t ipaddr;
struct
timer periodic_timer, arp_timer;
// Sys timer init 1/100 sec tick
clock_init(2);
timer_set(&periodic_timer, CLOCK_SECOND / 2);
timer_set(&arp_timer, CLOCK_SECOND * 10);
// Initialize the ethernet device driver
// Init MAC
// Phy network negotiation
tapdev_init();
// uIP web server
// Initialize the uIP TCP/IP stack.
uip_init();
// Init WEB server
uip_ipaddr(ipaddr, 192,168,1,100);
//printf(''IP Address: 0.100\n\r'');
uip_sethostaddr(ipaddr);
uip_ipaddr(ipaddr, 192,168,1,3);
uip_setdraddr(ipaddr);
uip_ipaddr(ipaddr, 255,255,255,0);
uip_setnetmask(ipaddr);
// Initialize the HTTP server.
httpd_init();
// Run WEB server and wait any key for exit
while
(1)
{
uip_len = tapdev_read(uip_buf);
if
(uip_len > 0)
{
if
(BUF->type == htons(UIP_ETHTYPE_IP))
{
uip_process(1);
/* If the above function invocation resulted in data that
should be sent out on the network, the global variable
uip_len is set to a value > 0. */
if
(uip_len > 0)
{
uip_arp_out();
tapdev_send(uip_buf,uip_len);
}
}
else
if
(BUF->type == htons(UIP_ETHTYPE_ARP))
{
uip_arp_arpin();
/* If the above function invocation resulted in data that
should be sent out on the network, the global variable
uip_len is set to a value > 0. */
if
(uip_len > 0)
{
tapdev_send(uip_buf,uip_len);
}
}
}
else
if
(timer_expired(&periodic_timer))
{
timer_reset(&periodic_timer);
for
(i = 0; i < UIP_CONNS; i++)
{
uip_periodic(i);
/* If the above function invocation resulted in data that
should be sent out on the network, the global variable
uip_len is set to a value > 0. */
if
(uip_len > 0)
{
uip_arp_out();
tapdev_send(uip_buf,uip_len);
}
}
/* Call the ARP timer function every 10 seconds. */
if
(timer_expired(&arp_timer))
{
timer_reset(&arp_timer);
uip_arp_timer();
}
}
}
return
(1);
} hello forum
I am new to TCP/IP
anybody who used uIP before can answer my question ?
this above is main body if uIP
how must I modify this code
so that it doesnot act as a webserver
but receives and sends back 200 or 300 bytes of data ?
thank you
#3rd-party #uip #uip #lwip
2013-04-09 8:59 AM
Hi ,
I want to know if you've found a solution for your probleme cuz i have the same problem. I want to ask u also about smthing, i've download Adam dunkel stack uIP and i have a serious problem, i used the simple application named '' hello world'' in apps directory and the uip_len always return 0 int main(void) { int i; uip_ipaddr_t ipaddr; struct timer periodic_timer; //struct uip_conn* conn; clock_init(); // Clock second =1000 timer_set(&periodic_timer, CLOCK_SECOND / 2); // Initialize the ethernet device driver network_init(); //Initialize the uIP TCP/IP stack uip_init(); //Init WEB server uip_ipaddr(ipaddr, 192,168,1,1); uip_sethostaddr(ipaddr); // // uip_ipaddr(ipaddr, 192,168,1,2); // uip_setdraddr(ipaddr); // // uip_ipaddr(ipaddr, 255,255,255,0); // uip_setnetmask(ipaddr); hello_world_init(); /* 4 test purpose conn=uip_connect((192,168,2,1), 1000); if(conn==0){ uip_abort(); return; }*/ while(1) { uip_len = network_read(); if(uip_len > 0) { uip_input(); /* If the above function invocation resulted in data that should be sent out on the network, the global variable uip_len is set to a value > 0. */ if(uip_len > 0) { network_send(); } } else if(timer_expired(&periodic_timer)) { timer_reset(&periodic_timer); for(i = 0; i < UIP_CONNS; i++) { uip_periodic(i); /* If the above function invocation resulted in data that should be sent out on the network, the global variable uip_len is set to a value > 0. */ if(uip_len > 0) { /* problem here */ network_send(); } } #if UIP_UDP for(i = 0; i < UIP_UDP_CONNS; i++) { uip_udp_periodic(i); /* If the above function invocation resulted in data that should be sent out on the network, the global variable uip_len is set to a value > 0. */ if(uip_len > 0) { network_send(); } } #endif /* UIP_UDP */ } } return 0;2013-04-09 11:30 PM
See:
http://e2e.ti.com/support/microcontrollers/stellaris_arm/f/471/p/155813/861350.aspx#861350
- and replace ''TI'' with ''ST''.The same applies to uIP.