STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Timer Prescaler Application Clarification

I did not understand the significance of the number 65536 in the below codepHandle->OvfFreq = (uint16_t)(pHandle->TIMClockFreq / 65536U); /* Set fixed to 150 ms */ pHandle->HallTimeout = 150U; /* Compute the prescaler to the closet value of th...

STuser2 by Senior III
  • 593 Views
  • 1 replies
  • 0 kudos

Official ST Example BSP for b-u585i-iot02a

I adapted the official BSP example code (available at https://www.st.com/en/embedded-software/stm32cubeu5.html, stm32cubeu5-v1-8-0.zip) to acquire and process audio. My code is running very slowly on the board. We thought the slowdown might be due to...

lucadelf by Associate II
  • 605 Views
  • 2 replies
  • 1 kudos

Resolved! Cannot make SPDIF TX work

Hello, I have made my own STM32F732RET6 board that has a USB FS configured as a Stereo, 24 bit 48kHz Audio Interface and SAI2 connected to an SN75176BDR (Differential Bus Transceiver IC) because I want to transmit AES3-AES/EBU (same as SPDIF) audio d...

post 1 clock 192mhz.png post 2 clock 3072mhz.png
nt2ds by Associate III
  • 3879 Views
  • 22 replies
  • 7 kudos