STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB (VCP) and EXTI together dont work

Posted on April 11, 2014 at 18:21Hello All,         I am using the STM32F4 discovery board. I am using USB as a VCP and EXTI for detecting the rising edge of my signal.        The USB and the EXTI work good when operated independently but don't work...

USB Mouse problem on STM32F105

Posted on April 14, 2014 at 11:13Hi to all! I need to work with USB mouse on F105 processor. I used latest USB host-device lib - STM32_USB-Host-Device_Lib_V2.1.0, little rework it: 1. Remove STM3210C-EVAL's display, I have my own display, different ...

hd44780 by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos

STM32F205RF with STM32CubeMX and USB

Posted on April 09, 2014 at 19:54HiI am fighting with USB again.Situation :STM32F205RF in NetDuino2 (schematic is here - http://netduino.com/netduino2/schematic.pdf)Code generated with CubeMX- first page : http://imtp.me/7ga902dr0- clock page : http...

voltr by Associate II
  • 1365 Views
  • 2 replies
  • 0 kudos

STM32F10x + FatFs issue

Posted on April 09, 2014 at 01:52 Hi All, I am new to this community so if I have posted this in the wrong place then please let me know. I have a STM32 Discovery board which I am trying to log data onto a SD card through SPI. I am...

Jump address to choose one of 2 binary in flash

Posted on April 03, 2014 at 17:49Hello, I'm trying to create a bootloader into the component STM32f106RDT with 384KO of Flash. I have mapped the memory like this: 0x08000000 - 0x0802DFFF for main software (first binary) 0x0802F000 - 0x08030FFF reser...

tommelou by Associate II
  • 5962 Views
  • 22 replies
  • 0 kudos

HID Report Descriptor Contains Wrong Byte

Posted on April 09, 2014 at 14:45I've got a USB HID device based on a STM32F427 that can be set up to run as either FS or HS USB. When I use FS, all is well. However, when I use HS (which uses the same descriptor), the report descriptor contains one...

jvavra by Associate III
  • 1324 Views
  • 2 replies
  • 0 kudos

STM32F3Discovery Problem with USB User

Posted on April 07, 2014 at 16:50Hi, I downloaded a USB device examples a I tried to use a Virtual Com Port Loopback.This example works only if I manualy replug usb cable when the program is started. Anyone knows how can I do software reset?I use a ...

slqa123 by Associate
  • 785 Views
  • 0 replies
  • 0 kudos

STM32F4 Discovery OTG FS Device Issue

Posted on April 06, 2014 at 10:09Hello Everyone,I am trying to send and receive data on STM32F4 Discovery over USB. USB is configured as Virtual Com Port (CDC) and running at full speed. STM32CubeMX is set up on my machine and the project that I hav...

emeydanli by Associate II
  • 1180 Views
  • 2 replies
  • 0 kudos