STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IAP with USB usage

Posted on April 30, 2014 at 10:39 Hello List, I have a working IAP program that uses USB to upload new code. See http://fwnhousing.rug.nl/stm-test for the code. The project IAPtest contains the code, including an example to u...

Sietse by Associate III
  • 1754 Views
  • 2 replies
  • 0 kudos

STm32Cube Input Capture bug

Posted on April 24, 2014 at 14:18 Hi, I would like to signal a bug using STm32Cube to configurate timers in InputCapture mode to measure the duration of an input signal resting at low level. Using the method described in AN4013 at page...

Virtual Com Port for STM32F103XC

Posted on April 07, 2014 at 12:44Hi Guys, I Am trying to port VCP Example Project found in STM32_USB-FS-Device_Lib_V4.0.0 on STM32F103XE Eval kit. Pin Description : PA12------USBDP-------Pulled up by 1.5K Resistor. PA11------USBDM PA10------USART1_R...

STM32cubef4 USB Virtual COM port

Posted on April 15, 2014 at 04:12Hello All,I found a few samples for USB Virtual COM port for STM32F4-Discovery board, but they are pretty old & not based on STM32CubeF4. Could anyone please hint me or direct me to a sample which has Virtual COM por...

harinath by Associate III
  • 2580 Views
  • 9 replies
  • 0 kudos

STM32F4 FreeRTOS UART interrupt

Posted on April 15, 2014 at 22:30 Using: STM32F407VGFreeRTOS 7.6.0 I am trying to read value of RFID card via UART interrupt. Problem is that data read by UART is somehow corrupted. If i don't use FreeRTOS this code works, which makes ...

zmayac by Associate II
  • 3850 Views
  • 7 replies
  • 0 kudos

STM32Cube - Barebone FreeRTOS + Lwip on F207

Posted on April 16, 2014 at 20:17Hello to all, I just set up a bare bone project for my F207VC custom board using the new STM32Cube. The board is tested and it is working perfectly with FreeRTOS 6.1.0 and Lwip 1.3.2. The used PHY is a Micrel KSZ8051...

abrous3d by Associate II
  • 3553 Views
  • 7 replies
  • 0 kudos