STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB CDC with flow control

Posted on February 19, 2015 at 08:25The example provided for Virtual COM over USB (STM32_USB-FS-Device_Lib_V4.0.0\Projects\Virtual_COM_Port) does not include UART flow control. The UART module is hard-coded to not use CTS/RTS, and when the UART-->US...

boaz by Associate II
  • 706 Views
  • 0 replies
  • 0 kudos

DMA Support in STMcube

Posted on January 30, 2015 at 15:53I am just integrating new STMcube for my project on STM32F4. I want to use DMA on USART1 without any interrupt. But i had a look at STMCube library, It uses Interrupts in DMA. Any thoughts  how can i make DMA work...

dhiry2k1 by Associate II
  • 1313 Views
  • 3 replies
  • 0 kudos

STM32F0 USB CDC Class from CubeMX

Posted on February 18, 2015 at 14:44Hey all,I'm trying to implement a USB CDC device on an STM32F072B-Discovery (uses the STM32F072RBT6 device) to simply send some values over to the serial console. I've not had much luck with this using the code ge...

Endless interrupts in VCP USB STM32L

Posted on February 12, 2015 at 13:23Hi, I use the USB VCP (based on VirtualComport_Loopback) in STM32L152VE. I disabled suspend (''__IO bool fSuspendEnabled = FALSE;'' in usb_pwr.c). If the USB cable is disconnected I get endless suspend interrups (...

igal by Associate II
  • 2195 Views
  • 4 replies
  • 0 kudos

stm32f4 reprogramming from externan nand memory

Posted on January 21, 2015 at 18:13Dear All, I know that the question about jumping to the bootloader of STM32 without boot0/1 has been answered many time especially by clive1. My goal is to reprogram STM32F4 from the attached external NAND memory (...

davhak by Associate II
  • 3597 Views
  • 9 replies
  • 0 kudos

Using internal flash memory as FatFs drive

Posted on February 13, 2015 at 13:56 I'm trying to make internal flash on STM32F051xx to be seen as a drive. This is the code on the top level: char USER_Path[4]; /* USER logical drive path */ FATFS USER_FatFs; /* File syste...

dscdsc by Senior
  • 3434 Views
  • 5 replies
  • 1 kudos

Ethernet Over USB

Posted on June 27, 2013 at 20:14Has anyone seen any code to do Ethernet Over USB from an STM32? I'm looking for something similar to how the BeagleBone boards work. When you plug their USB into Windows (and have the right drivers) they show up as a ...

CMSIS SPI Driver wait forever in SendData function

Posted on February 11, 2014 at 14:00 Hi all, I'm trying to use the SPI interface on a STM32F207 with CMSIS. Below you my sample code can be seen. The problem there is that within the function drv_Info->SendData(...) the function wait...

b_ by Associate II
  • 2653 Views
  • 5 replies
  • 0 kudos

stm32f103c8 spl can, no tx impulse

Posted on February 11, 2015 at 07:01 Please, help me, i cant start CAN for a week. I use stm32f103c8 + mcp2551, connected to car can bus. Receiving is working, i got packets in irq. But transmit is always pending. All mail boxes becomes pendi...

aneox by Associate
  • 1066 Views
  • 1 replies
  • 0 kudos