cancel
Showing results for 
Search instead for 
Did you mean: 

USB CDC with flow control

boaz
Associate II
Posted on February 19, 2015 at 08:25

The example provided for Virtual COM over USB (STM32_USB-FS-Device_Lib_V4.0.0\Projects\Virtual_COM_Port) does not include UART flow control. The UART module is hard-coded to not use CTS/RTS, and when the UART-->USB buffer overflows, the head pointer is set to 0, running over previous data:

hw_config.c:

bool USART_Config(void)

{

...

...

USART_BaudRate = linecoding.bitrate;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

 

/* Configure and enable the USART */

STM_EVAL_COMInit(COM1, &USART_InitStructure);

return (TRUE);

}

void USART_To_USB_Send_Data(void)

{

  

...

USART_Rx_Buffer[USART_Rx_ptr_in] = USART_ReceiveData(EVAL_COM1);

...

  

USART_Rx_ptr_in++;

  

/* To avoid buffer overflow */

if(USART_Rx_ptr_in == USART_RX_DATA_SIZE)

{

    USART_Rx_ptr_in = 0; // <-- no flow control

}

}

Questions:

  • Is there a sample code which does implement UART flow control?
  • How should the example code be modified to support this?
  • Will switching to Cube's HAL help in this case?

#usb #usart #flow
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0