STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBX host on USB-A of STM32N6570-DK

Hi,I tried to bring up the USB host on the USB-A connector, but without success.As a starting point, I took the example project:STM32CubeN6\Projects\STM32N6570-DK\Applications\USBX\Ux_Host_DualClass (for the USB Type-C connector), replaced USB1 with ...

ERROR by Senior
  • 960 Views
  • 4 replies
  • 2 kudos

Usb device MSC problem

 I'm already achieved a USBX-MSC class, and also a FileX in MCU local.I know that using two file systems at the same time is not recommended, but still have some questions. 1. I implement the ux_deveice_msc.c as followed. Use PC-Windows to create a f...

Jason927 by Associate III
  • 644 Views
  • 3 replies
  • 0 kudos

Resolved! Bare metal USB HID

Hello,I am trying to implement a USB HID keyboard on an STM32F042 without HAL or LL, just simple register defs. I took an example code generated in CubeIDE with HAL and a few other examples. I extended the example with HAL to also implement the LEDs ...