2025-09-11 12:53 AM - last edited on 2025-09-11 1:53 AM by mƎALLEm
ST moderator: Thread moved from "STM32CubeIDE" forum to "STM32 MCUs Embedded software" forum.
Hello,
I am currently working on STM32H755 (dual-core M7/M4) and trying to use the FMC interface to connect to an external SRAM.
I have checked the STM32CubeH7 firmware package, but I could not find any ready-made FMC SRAM example for STM32H755 (most examples for STM32H745).
I have checked the STM32CubeH7 firmware package,
and it seems that for STM32H745 (and STM32H755) there is only an FMC SDRAM example available,
located under: STM32CubeH7\Projects\STM32H745I-DISCO\Examples\FMC\FMC_SDRAM_DataMemory
Could you please provide:
An official or working example project for STM32H755 FMC SRAM
Clarification about which core (M7 or M4) should configure the FMC?
Best regards,
Allen
Solved! Go to Solution.
2025-09-11 1:35 AM
Hello @HAL_Allen and welcome to the community,
1- You can refer to that example from github: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/FMC/FMC_SRAM No official example
Unfortunately, no official example with with STM32H755
2- Both cores can initilize/use FMC.
2025-09-11 1:35 AM
Hello @HAL_Allen and welcome to the community,
1- You can refer to that example from github: https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H743I-EVAL/Examples/FMC/FMC_SRAM No official example
Unfortunately, no official example with with STM32H755
2- Both cores can initilize/use FMC.
2025-09-15 7:58 PM
Hello,
Thank you for your reply and guidance, I understand the issue now. Really appreciate your help!