STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multichannel ADC

Posted on May 06, 2015 at 19:17 Hi, I'm developing application on STM32F0 where I use two gas sensors (CO and CO2), so I need two channels on ADC. In my main.c I only call two functions and on beginig of each function I change channel like so: ...

muliku by Associate II
  • 5154 Views
  • 10 replies
  • 0 kudos

STM32 Touch Sensing Library Example Touchkey

Posted on May 12, 2016 at 01:02I am looking for any example of TouchKey application on any STM32 using Touch Sensing Library. Preferably using code generated by STM32CubeMX. Anyone? Any clue? Thank you. #stm32-cube-touch-sensing-library

ekawahyu2 by Associate II
  • 1154 Views
  • 1 replies
  • 0 kudos

Virtual Comport Driver

Posted on April 08, 2016 at 07:21Hi. we are using the VCP1.4.0 Driver to use STM32F042 USB SERIAL. But , in the Windows 10, driver happen some strange behavior. For example, when we disconnected the usb port, Windows CPU load goes up suddenly. So we...

yymo1019 by Associate II
  • 1830 Views
  • 3 replies
  • 0 kudos

STM32L476 had too much coffee

Posted on May 06, 2016 at 22:49I have been trying to implement the Tickless Idle feature in FreeRTOS (which comes pre-implemented for STM32 processors).In my main code I have turned off all IP except the pushbutton (EXTI0), which I want to use to wa...

mattreed9 by Associate III
  • 1155 Views
  • 1 replies
  • 0 kudos

Stuck in HAL_I2SEx_TransmitReceive_IT because Interrupts called immediately but not handled as I2S_HandleTypeDef is still locked

Posted on May 10, 2016 at 09:10Hi all,I encountered a problem, using version 1.4.4 of the I2S Hal module driver in Master TX full duplex mode. Basically I'm just writing a test program to see that it works, the idea is to transmit data and connect t...

BOOT0/BOOT1 pins - boot mode doubt

Posted on May 09, 2016 at 13:14Hello all.I have a little doubt about BOOT0/BOOT1 pins, they select the boot mode.After reading about in some pages, I understood that ''System memory boot'' selects the builtin bootloader to write a new firmware using...

0690X00000605O2QAI.png
jeferson by Associate II
  • 28493 Views
  • 5 replies
  • 0 kudos