cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX ethernet of clean generated code chrashes (lwIP FreeRTOS STM32F4)

lau_di
Associate
Posted on February 19, 2016 at 09:47

After compiling the CubeMX generated Code (without any changes).

The Ethernet stack crashes if it receives many UDP-packages in a short time. (1000-10000 10Byte packages in a few ms)

Even after stopping the flood the interface never comes up again.

The interface only comes back again if I call ''static void low_level_init(struct netif *netif)'' (without creating the thread and semaphore again) or after a software reset.

This behaviour is really bad.

Could you help me?

uC: STM32F437IITx

PHY: DP83848

CubeMX 4.13.0 (Firmware Package for Family STM32F4 1.11.0):

- FREERTOS

   - [x] Enabled

- LWIP

   - [x] Enabled

- ETH:

   - Mode: MII

   - [ ] Activate Rx Err signal

- RCC:

   - High Speed Clock (HSE): Crystal/Ceramic Resonator

   - Low Speed Clock (LSE): Disable

   - [x] Master Clock Output 1

   - [ ] Master Clock Output 2

   - [ ] Audio Clock Input (I2S_CKIN)

- SYS:

   - Debug: JTAG (5 pins)

   - [ ] System Wake-Up

   - Timebase Source: TIM6

  

ETH_COL is sticked to pin PA3.

LWIP settings:

- IP_ADDRESS (IP Address): 192.168.001.049

- NETMASK_ADDRESS (Netmask Address): 255.255.255.000

Another error, which has nothing to do with the upper one, is (stm32f4xx_hal_conf.h):

&sharpdefine PHY_MICR_INT_OE                 ((uint16_t)0x0002U)  /*!< PHY Enable output interrupt events              */

It should be:

&sharpdefine PHY_MICR_INT_OE                 ((uint16_t)0x0001U)  /*!< PHY Enable output interrupt events              */

#freertos #lwip #stm32f4
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on February 24, 2016 at 14:52

Hi di.lau,

The issues are reported internally to be checked by CubeMX team.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

lau_di
Associate
Posted on March 03, 2016 at 15:18

Do you have some new information?

stm32cube-t
Senior III
Posted on May 11, 2016 at 11:37

Dear user,

Please upgrade to next version 4.15 (available soon) that will fix these issues.

Best regards