STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NucleoF103, CubeMX HAL, PWM Out Tim3CH1

Posted on May 04, 2016 at 22:50hi im working on a project to drive a WS2812B led string. i use TIM1 as time source and TIM3 for the PWM generation. im so far able to achieve a PWM signal @ 800kHz. For testing, i tried (see stm32f1xx_it.c) to drive ...

aal1 by Associate II
  • 4248 Views
  • 9 replies
  • 0 kudos

STM32F107 CAN bootloader many faulty messages

Posted on November 15, 2013 at 16:01The native CAN bootloader of STM32F107, revision Z, date code 244, produces many faulty messages. Peak CAN controller to communicate with the bootloader via CAN reports various errors as RX frame, TX frame errors,...

tannert by Associate
  • 2458 Views
  • 4 replies
  • 0 kudos

BOOT DFU USB with STM32F427 dont work

Posted on May 04, 2016 at 01:53Hello:I have develop a board where may install STM32F407, STM32F405 or STM32F427. Board is always same, and work perfect with F405 and F407 about the BOOT option to upload firmware by DFU USB.But when I install an F427...

pinballsp by Associate II
  • 2974 Views
  • 6 replies
  • 0 kudos

STM32F4 - Jump from Boot to App

Posted on May 05, 2016 at 12:37Hey guys, my first step in creating a bootloader was simply to move the app (which resided at 0x8000000 to 0x8020000 through the linker file. Next, I created a basic bootloader at address 0x8000000 which basically does...

bdesantis by Associate II
  • 2553 Views
  • 4 replies
  • 0 kudos

STM32L4 default DFU mode verus Standalone

Posted on August 05, 2015 at 17:25We used the DFUSE over USB successfully with several L152 designs. The L152 chips don t have a USB boot loader DFU like described in the AN2606 STM32 microcontroller system memory boot mode. (DFU SE via USB) So we d...

uwe2 by Associate II
  • 10311 Views
  • 29 replies
  • 0 kudos

Set a RTOS Uart queue with the HAL librarie

Posted on May 02, 2016 at 11:11Hi everyone, I would like to include in my project  FreeRTOS a uart queue. I have already  done this with the StdPeriph lib but I'm facing difficulties to migrate from StdPriph to HAL. My previous project was build l...

dauphin2 by Associate II
  • 2862 Views
  • 4 replies
  • 0 kudos

STM32F103VE USB Mass storage speed issue

Posted on April 27, 2016 at 10:55Hi,My application includes USB with mass storage class, I am using STM32F103VE MCU running at 72Mhz. Sandisk uSD(8GB, Class 10) used with SDIO  interface.I have used USB MSC code from STM32F1 library (STM32_USB-FS-De...

K_K by Associate III
  • 2210 Views
  • 5 replies
  • 0 kudos