STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Aid with HAL library

Posted on July 25, 2015 at 16:09Hello there, I am trying to make my way into hal library and stm32 but I find it very difficult. The files seem to be well documented with the doxygen, but it doesnt help me much. Is there any tutorial or a book even ...

Retrieving CAN frames in interrupt (HAL)

Posted on July 24, 2015 at 15:43Hello there, I am using STM 32F4 cube to generate code for my application (stm32f4discovery board). I Can succesfully send can messages using: /* CAN message to send */   CanTxMsgTypeDef TxMess;   TxMess.ExtId = 0x234...

CAN BUS, cube not receiving message

Posted on February 07, 2015 at 13:10Hello, I have been using standard libraries but when CUBE got released I switched. I cant receive any CAN messages with CUBE.-I am using f072-Configured clocks, baud rate, filters(default)-Using interrupt-Silent l...

laggersvk by Associate II
  • 2237 Views
  • 8 replies
  • 0 kudos

STM32F070 Nucleo UART2 Not working EIE=1

Posted on July 21, 2015 at 15:16 I new to STM cubemx through which I have generated code for AC6 Nucleo stm32f070 for simple uart transmission and reception. I saw a video and made the code main code following /** ********************...

gada by Associate III
  • 613 Views
  • 1 replies
  • 0 kudos

STM32F4 SDIO continuos stream

Posted on July 23, 2015 at 11:02 Hi, For the past few days I have been trying to get data written to an SDHC card at a constant rate of 1.2MBps without any success. I have based my SDIO driver on Clive's example, which was posted somewhere e...

felipe2 by Associate III
  • 521 Views
  • 0 replies
  • 0 kudos

Audio Middleware in STMCube

Posted on July 21, 2015 at 21:30Dear STMCube developers, it's a great pleasure to use the STMCube software. Still, the tool seems to be raw (or perhaps I haven't completely mastered it). I want to use Audioplayer middleware in my project based on ...

sdobrets by Associate
  • 599 Views
  • 0 replies
  • 0 kudos

Writing to External SPI Flash using DfuSe (USB)

Posted on July 20, 2015 at 15:27Hello Guys, Please, could you tell me whether it would be possible to write binary data to an External SPI Flash from DfuSe (USB)? I have a custom board with stm32f427. There is an SPI Nor Flash connected to the micro...

ouzenkov by Associate
  • 660 Views
  • 1 replies
  • 0 kudos

STM32F4 Discovery won't go into DFU bootloader mode

Posted on July 18, 2015 at 00:19Hi All,I have two discovery boards. When I go into discovery mode (boot0 high, boot1 low)  and then run ''dfu-util -l''  ... with one board I see the devices listed, the other board not .. could this be a faulty board...

bmentink by Associate II
  • 1284 Views
  • 3 replies
  • 0 kudos