STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash STM32F103 via SPI

Posted on October 09, 2015 at 16:22Hi,i have an application with an STM32F103 and a Raspberry Pi, connected via full duplex SPI.I want to implement automated flashing of the STM. The idea is:RPi contacts STM32 via SPI and if STM32 does not answer or...

STM32F0 hardfault error with HAL Library

Posted on October 09, 2015 at 15:34 Hello We are currently switching from the STD library to the HAL library. Personally I'm not very pleased with that, but due to upcoming projects with F7 MCU we are mandatory to learn to use the HAL Lib...

mvugs9 by Associate II
  • 804 Views
  • 2 replies
  • 0 kudos

USB Device function on the STM32Cube

Posted on October 02, 2015 at 05:14Hi, I'm making CDC device function on the STM32Cube and STM32F4Discovery. (Using STM32CUBEMX) But the USB communication between above and PC(Windows 7 32bit) is interrupted as ''STALL'' after GET_DESCRIPTER(DEVICE ...

STM32Cube_FW_F0_V1.3.0 BUG report/fix

Posted on September 22, 2015 at 21:55Channel ADC_CHANNEL_VREFINT  does not work because it is not enabled in the register CCR --- STM32Cube_FW_F0_V1.3.0/Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_adc_ex.h.orig 2015-06-25 23:53:50.000000000 +0300...

stm by Associate
  • 730 Views
  • 2 replies
  • 0 kudos