Delay after Write Memory for STM32F429 SPI bootloader
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-10-01 7:41 PM
I have most of the commands implemented for the STM32F429 SPI bootloader, but Write Memory is not working. The documentation says that a delay is needed after the length, data, and checksum are provided, before requesting the ACK, but I cannot find the appropriate table with that information. I have found tables for the Erase times, including 16 KB sectors and up. However, since the ST bootloader Write Memory command takes, at most, 256 bytes, I don't see a way to determine the delay needed.
I've tried 4096 us (4.096 ms), but I still get NAK.Any idea? #write-memory #flash #bootloader- Labels:
-
Bootloader
-
Flash
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-10-05 10:26 AM
Does no one have information on the correct delay time for 256-byte Flash writes on the STM32F429?