STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F756 USB and WFI

Posted on July 27, 2017 at 09:55I have a problem with STM32F756 USB CDC (HS with FS PHY) device and core sleeping. I isolated all other code and left only the USB driver and main loop calling WFI instruction. If there is no call to WFI, USB is worki...

Any reason not to use CAN identifier as node ID?

Posted on July 31, 2017 at 02:17Preamble for the uninitiated:CAN identifiers are usually associated/related with/to the content of the message rather than as an identification mechanism for a specific participant on the bus.The question therefore:In...

connect by Associate II
  • 2881 Views
  • 3 replies
  • 0 kudos

stm32l053 USB VCP not getting detected

Posted on July 29, 2017 at 11:14Hi,                 I'm currently working on stm32l053 VCP. I've done a code to initialize & start VCP driver in stm32l053 and tested it using stm32l053-DISCO board, where it works fine. I can able to detect the com p...

0690X00000607jmQAA.png
LRPS_92 by Associate II
  • 1337 Views
  • 2 replies
  • 0 kudos

HAL_UART_Transmit_IT pauses during transmission

Posted on July 28, 2017 at 22:16Hi everyone,This is not a very serious issue for my application, however, I would like to understand this behavior.In my application, when the STM receives a packet, it sends out a packet with a confirmation. The cont...

0690X00000607jgQAA.png 0690X00000607gYQAQ.png 0690X00000607jMQAQ.png
Lucas C by Associate II
  • 1838 Views
  • 3 replies
  • 0 kudos

Resolved! Development boards to use for FreeRTOS and ThreadX

Posted on July 28, 2017 at 21:48We are currently trying to port an application from Linux to ThreadX and FreeRTOS and wanted feedback from the community on which development boards would you recommend to use. Looking for a board with Cortex-M proces...

CubeL4 missing CMSIS

Posted on July 14, 2017 at 10:21Hi!I've migrated one of my projects to CubeL4 v1.8.1 and regenerated my configuration using CubeMX. After that, my project did not compile and I noticed that the cmsis drivers were missing. After a bit of investigatio...

USB Huawei modem with stm32f407

Posted on July 26, 2017 at 10:04Hi,I'm working on application that uses a USB HUAWEI MU709 modem with STM32F407. First off all, i used the usb stack from keil to  implement the CDC mode: https://www.keil.com/pack/doc/mw/USB/html/host_cust_tutorial.h...

hilwan by Associate II
  • 1495 Views
  • 2 replies
  • 0 kudos

USB CDC and MSC Middlewares integration

Posted on July 27, 2017 at 13:13Hi all, I'm using STM32L486 microcontoler and USB device. Using MSC_Standalone and CDC_Standalone project example from the STM32Cube I was able to configure the USB device on CDC and MSC. Now, I want to integrate both...