STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bug in USB HID code

Posted on May 28, 2017 at 12:46I'd like to report a bug.In the file usbh_hid_keybd.h, line 118:&sharpdefine KEY_CAPS LOCK                          0x39should be replaced with:&sharpdefine KEY_CAPS_LOCK                          0x39#usb #hid #keyboar...

Flashing STM32L011F3P bootloader

Posted on March 02, 2017 at 11:26Hello everybody,I would like to make my first program on the PCB that I have soldered with a STM32L011, but I can't upload my first program. You can help me.I am the instructions of this forum, but I have no boot1 on...

ibrahim by Associate II
  • 3161 Views
  • 6 replies
  • 0 kudos

STM32 Timer interrupts immediately after start

Posted on September 29, 2017 at 00:33i don't know if it's a feature or bug, but starting a timer in interrupt mode will bring the code into the interrupt handler the first time mcu calls timer start function.To solve this problem it's enought to cle...

CubeMX F0 1.8 issues

Posted on May 17, 2017 at 09:58Hi!For me, the new 1.8 version of CubeF0 is completely broken. Using the HAL RCC driver, it tries toa) enable USART2 that I don't use, and it fails because it can't set its clock sourceb) enables HSI oscillator (which ...

STM32F070CB HAL SPI2 RX interrupt

Posted on September 27, 2017 at 19:16   I am trying to setup and run  SPI2 RX interrupt on a STM32F070CB microcontroller. I am utilizing the STM HAL drivers to setup the SPI and I am using  the STM32CubeMX to setup the code for my project. I am tran...