STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 I2c1 and USART1 (and USART6) conflict

Posted on October 14, 2017 at 19:32I have an STM32F446RE Nucleo board. I am using I2C1 in interrupt (not DMA) mode, to continuously read data from an MPU9250 accelerometer/magnetometer/gyroscope board. I also use the USART1 to read logs with my lapt...

STM32F765BIT MCU ethernet problem.,

Posted on October 09, 2017 at 16:47Hello ., I am working with STM32F765BIT MCU in our custom board. In this I need to make Ethernet interface working with any of protocol (like UDP).I have generated code using STM cube , but I am not sure that I am ...

STM32CubeMX 4.20 BugReport (ADC Dual Mode)

Posted on March 31, 2017 at 03:51I'm using STM32CubeMX 4.20 and STM32CubeF1 v1.4.0 HAL driver. There is a bug when you configure the ADC1 as dual regular simultaneous mode. The code generator adds multi-mode configuration for both ADCs (master and s...

STM32F107 UART Interrupt issue with HAL

Posted on October 10, 2017 at 00:18Hi,I've a question regarding the HAL UART Environment. I could observe that the Interrupt are raised sometimes 2x although  I'm sending only one Byte for the STM32 where I'm reading each single byte.At which condit...

DfuseDemo on Ubuntu using Wine

Posted on September 29, 2017 at 12:53Hi ,       I am using DfuseDemo for flashing .dfu on to my stm32l476 based board. This is working fine in the windows 7 environment. But , now to build my code i switched linux ubuntu, so i tried installing the D...

Madhu R by Associate II
  • 2309 Views
  • 2 replies
  • 0 kudos