STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 Standard Peripheral Libraries

Posted on November 08, 2017 at 09:37Hello,  Are the Standard Peripheral Libraries available for L4 series? If not, maybe it is possible to use StdPeriph from e.g. F4? Register addresses are the same or not? Maybe there is some way to extract it fr...

Kaza K by Associate II
  • 4757 Views
  • 8 replies
  • 0 kudos

RTX Critical Sections

Posted on November 08, 2017 at 08:46Hi,I am trying to port a code that is working with FreeRTOS to RTX. The microcontroller is the same: STM32F4.The code uses critical sections. I have tried using the same implementation for the critical section for...

andrei by Associate II
  • 880 Views
  • 0 replies
  • 0 kudos

STM32L4 USB CDC (VCP) Max packet transfer

Posted on January 26, 2017 at 11:29On investigating the use of the USB device drivers provided for the STM32Lx series chips (CDC) I found an issue when trying to transfer a packet to the PC which is an exact multiple of 64 bytes. In such a case the ...

Ant M by Associate II
  • 1742 Views
  • 2 replies
  • 0 kudos

USB MSC device implementation on Sensortile

Posted on November 05, 2017 at 23:00Hi,I am trying to implement USB  mass storage device class on the Sensortile which uses STM32L476. I used the sample audio loop  app to verify that USB works fine. However, when I ported the MSC device functions f...

Bala K by Associate
  • 1083 Views
  • 1 replies
  • 0 kudos

STM32 USB Library for WinUSB

Posted on April 10, 2012 at 04:57Does anyone have a demo /  tutorial on how to setup the STM32 USB Library to work with the WinUSB driver.  Jan Axelson's ''USB Complete Fourth Edition'' describes how to setup the descriptor, and how to setup the INF...

Stephen28 by Associate III
  • 8072 Views
  • 12 replies
  • 0 kudos

STM32CubeMX generated code doesn't work?

Posted on November 03, 2017 at 22:21Hello.I want to implement USB-CDC device on STM32F070P6. I've generated the needed code using STM32CubeMX but it doesn't seems to work.I can't see USBD_CDC_Init to be called, thus when the device is flashed I get ...

Transfer data from PC to STM32 using USB HID

Posted on November 03, 2017 at 20:15Hi there,I've developed a USB HID mouse with the STM32F103C8T6 using STM32CubeMX and Keil uVision 5.Everything works fine so far (I've used the default mouse descriptor generated by CubeMX).But now, I've added a L...

STM32F1 reboots with new FreeRtos v9

Posted on November 03, 2017 at 08:54Hi there,I using a STM32F103 in my project and I generate the Keil project with Cube32MX with this firmware package for STM32F1 version 1.4.0.Today I update the Cube to version 4.23.0 and I migrate my project (inc...

Fede Rico by Associate III
  • 722 Views
  • 0 replies
  • 0 kudos