STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 DHCP Error

Posted on December 22, 2017 at 17:35I am using the STM32H743 NUCLEO-144, CubeMX V4.23.0, and CubeH7 V1.1.0.I do not see how DHCP can ever work using the CubeMX generated code. At the end of MX_LWIP_Init() is the only place where dhcp_start() is call...

MDS by Associate III
  • 927 Views
  • 0 replies
  • 0 kudos

Bug in USB HID, keyboard code

Posted on July 13, 2017 at 11:18I'd like to report a bug. In the file usbh_hid_keybd.c, ver. V3.2.2, date: 07-July-2015line 333:Now is: if(HID_Handle->length > (sizeof(keybd_report_data)/sizeof(uint32_t))){    HID_Handle->length = (sizeof(keybd_repo...

How to change USBH_malloc

Posted on November 06, 2017 at 15:59Hello,I`m using the CubeMX 4.23 and want to use the HAL USB Driver. In the usbh:conf.h is the code:/* Memory management macros */ &sharpdefine USBH_malloc malloc&sharpdefine USBH_free free&sharpdefine USBH_memset ...

tekampe by Associate II
  • 1780 Views
  • 3 replies
  • 0 kudos

Resolved! LwIP UDP updated examples ?

Posted on June 28, 2017 at 16:42Hello fellow stm32 explorersI am currently trying to communicate on a LAN network between a pc (server) and my stm32F4 discovery + phy module (client) via a UDP protocol.I am using LwIP with the RAW api (also called N...

andy b by Senior
  • 8378 Views
  • 3 replies
  • 0 kudos

Get serial port buffer size

Posted on December 18, 2017 at 08:14Hi All,   I'm using FreeRTOS and NUCLEO-F746ZG. Is there a way to get the size of the serial port buffer memory? The only way that I found is using register but I'm looking for a better solution.@arg UART_FLAG_RXN...

USB VIRTUAL COMM (WDF_VIOLATION) on the STM32F4

Posted on December 19, 2017 at 19:50I am working with the HAL library with cube as the code generator. I am using the USB virtual comm and it seems it was working fine in the beginning; however, when I am transferring a a lot of data my PC will some...

cleonb322 by Associate III
  • 705 Views
  • 0 replies
  • 0 kudos

[STM32F407] CS43L22 problem!

Posted on December 16, 2017 at 02:40Hello!I am working with CS43L22 on STM32F407VG Discovery Board. I use Audio_playback_and_record example to play .wav file. If i use headphone, I can get good sound. But If I use speaker I get small sound. Is that ...

STM32 Microcontroller USB interface

Posted on December 18, 2017 at 15:17Hello.,I am working with STM32F7 MCU in custom board, Actually it has two onboard MCU(both are STM32F7 microcontroller), Now my first task is to establish USB communication between two MCU's . I tried by configuri...

STM32CubeF0 - SPI functions problem

Posted on July 13, 2016 at 09:27Hi All,We are using STM32F072B and faced with SPI comm. problem.I have seen that Cube SPI functions have some bugs. HAL_SPI_Receive does not reading first three byte and loosing last three byte. I have seen several bu...

0690X00000602xaQAA.jpg 0690X000006036gQAA.jpg