STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I start task inside task on RTOS ?

Posted on April 02, 2017 at 09:52Everyone,Can I start task inside task on RTOS? so after task 1 is finished, go to task 2, finish task 2 return to task one,Here's what I have written, any advices ?thanks/* StartDefaultTask function */static void Sta...

How to write to USB PHY ULPI register ?

Posted on April 01, 2017 at 09:25Hello, how do you write to an USB PHY configuration register via ULPI ? I would like to swap DP and DM pins from Microchip USB3343 by setting bit 1 of register 0x39. http://ww1.microchip.com/downloads/en/DeviceDoc/33...

[bug report] Bug in HAL (SPL) delay function

Posted on March 12, 2014 at 16:05Setup: I've just generated code for stm32f407 using the latest STM32CubeMX. Here's the generated code for delay function in file stm32f4xx_hal.c:void HAL_Delay(__IO uint32_t Delay) {   uint32_t timingdelay;     tim...

amomum by Associate III
  • 2734 Views
  • 13 replies
  • 1 kudos

printf with HAL_UART_Transmit_IT?

Posted on November 09, 2016 at 10:34 I am new to the hal libraries (but not stm32 devices) and struggle to see howHAL_UART_Transmit_IT is expected to be used for something simple like printf over uart. Take a blocking example: void...

toby2 by Senior
  • 10110 Views
  • 30 replies
  • 0 kudos

stm32cube plugin for qtcreator

Posted on May 03, 2014 at 13:19Hello, I think I have a problem similar to the one described in the post ''STM32CubeMX as Eclipse plugin on Linux 64 machine''. As I'm really reluctant to use eclipse, I would like to know if a plugin for Qtcreator is ...

Resolved! FreeRTOS and SDIO setting ?

Posted on March 24, 2017 at 14:38Everyone,I tried to run SDIO with RTOS, but never got luck,Any ideas why ?If I disabled RTOS, SDIO can run properly but if I enabled it, SDIO is stopped running..Thanks#freertos #sdio

Debug problems with STM32F030

Posted on March 26, 2017 at 21:35 Hello. I'm trying to debug code on STM32F SWD debug wire is enabled. I can get into debug mode! The problem is that the code blocks whenever a HAL_Delay() occurs. I think the problem is related to systick...

USART bootloader protocol firmware

Posted on March 26, 2017 at 10:33Good day!There is 'http://www.st.com/content/ccc/resource/technical/document/application_note/51/5f/03/1e/bd/9b/45/be/CD00264342.pdf/files/CD00264342.pdf/jcr:content/translations/en.CD00264342.pdf'. And as I understa...