STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX F4 1.16 Firmware

Posted on April 24, 2017 at 04:17Hi everyoneMy cubeMX try to update the firmware of F4 to 1.16 but it failed as it used to.So I try to download the firmware here in ST website.But after I download the zip file which said 1.16 on the website but actu...

Jerry Lin by Associate II
  • 1804 Views
  • 7 replies
  • 0 kudos

USB CDC VCP device flow control?

Posted on December 06, 2016 at 15:36The function CDC_Receive_HS() is not meant to be exited until all data is copied from the USB stack.Is there a way to not do this? I am not using an operating system, so not leaving the function means blocking eve...

Resolved! STM32L4 + Timer IT + µs counter

Posted on April 24, 2017 at 17:30Hi All,I'm using STM32L486RG microcontroler, And 1Wire EEPROM.I have to use Timer to compute delays type ( delay for 5 �s to 500 �s).And I'm asking on How to Re-configure Timer on it's interrupt callBack and restart ...

Resolved! Fatfs Stack and Heap Memoty Requirement

Posted on April 24, 2017 at 12:28Hi, there!First time developing Fatfs with lovely STM32F091 Nucleo board. Have some serious memory problems here.-----------------------------------------------------------------------------------Hardware: STM32F091 ...

Zt Liu by Senior III
  • 2316 Views
  • 6 replies
  • 0 kudos

while (ETH->DMABMR & ETH_DMABMR_SR) HANGS

Posted on December 07, 2016 at 16:03Hi.This above code (part of the procedure PowerControl(..)) runs OK on my MCBSTM32C (KEIL evaluation) board.But, when the same code is loaded to my target system, the SR-bit (Software Reset) of the ETH_DMABMR is a...

Option Byte Loading (OBL_LAUNCH) fails

Posted on April 22, 2017 at 13:10Hi, I'm having an issue on STM32L151RC with HAL_FLASH_OB_Launch(), simplifying:if (HAL_FLASH_OB_Unlock() == HAL_OK){    HAL_FLASH_OB_Launch();    while (1);}MCU seems to fall in an undefined state.Certainly GPIO peri...

elKarro by Associate III
  • 1486 Views
  • 1 replies
  • 1 kudos

STM32F103 ADC and timer interupt

Posted on April 19, 2017 at 20:11Hello!I want to build a project where i need to do about 3500 readings from a CCD sensor in a short period a time. The signal i want to read has a frequency of about 0.35MHz, which should be fine as long as i use  13...