STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L432KC - I2C1 Not Working

Posted on June 23, 2018 at 06:30Hello,My team and I have been having troubles using the HAL drivers with I2C1. We are attempting to use PA9 and PA10 as our I2C1_SDA and SCL pins, but noticed that PB5 and PB6 are also listed as I2C1_SDA and SCL pins....

Buffer overflow in CubeMX SDMMC-Driver

Posted on May 30, 2017 at 18:11I'm trying to get a SD-Card working with FATFS on a NUCLEO-L476RG. Code was generated with recent STM32CubeMX 4.0 and Firmware Package 1.8.0 for L4. SD-access in polling mode, no DMA.My application was crashing (Defaul...

DFU error: bad state machine in firmware

Posted on May 18, 2018 at 14:17Hello Everyone,I am have a problem using Dfuse (v3.0.5) with my STM32L432KC.I have a USB CDC class, not using a composite CDC-DFU.Performing the DFU mode through the boot pin/bit.During upgrade I got the following erro...

0690X0000060BHqQAM.png
flo flo by Associate II
  • 3010 Views
  • 6 replies
  • 0 kudos

LwIP: link always down

Posted on June 21, 2018 at 16:53I have a problem using the LwIPIf I have a project where there is only the LwIP, everything works.MX_GPIO_Init(); MX_LWIP_Init(); httpd_init(); myCGIinit(); while (1) {    MX_LWIP_Process();}If I add something else (...

Rick MC by Associate III
  • 1358 Views
  • 1 replies
  • 0 kudos