STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Timer interrupts immediately after start

Posted on September 29, 2017 at 00:33i don't know if it's a feature or bug, but starting a timer in interrupt mode will bring the code into the interrupt handler the first time mcu calls timer start function.To solve this problem it's enought to cle...

CubeMX F0 1.8 issues

Posted on May 17, 2017 at 09:58Hi!For me, the new 1.8 version of CubeF0 is completely broken. Using the HAL RCC driver, it tries toa) enable USART2 that I don't use, and it fails because it can't set its clock sourceb) enables HSI oscillator (which ...

STM32F070CB HAL SPI2 RX interrupt

Posted on September 27, 2017 at 19:16   I am trying to setup and run  SPI2 RX interrupt on a STM32F070CB microcontroller. I am utilizing the STM HAL drivers to setup the SPI and I am using  the STM32CubeMX to setup the code for my project. I am tran...

problem with usb device cdc in hal library

Posted on September 26, 2017 at 17:56Hello, allI recently learn to use stm32 usb deviceI think it's easy to build a CDC example with HAL library in CubeMX,And I put the code into stm32f429-discvoery, it's the HS pin, but actually use FS speedI'm suc...

ctc.ctc by Associate II
  • 1471 Views
  • 4 replies
  • 0 kudos

STM32 Error Driver HAL_StatusType Def not found

Posted on September 26, 2017 at 17:43Hello,I am experiencing some problems when I set up the STM32L432KCU6 NUCEO-L432KC wiith FreeRTOS. The driver files containing HAL are causing compilation errors (see attached screenshots) when used in eclipse.Wh...

F K by Associate II
  • 1876 Views
  • 4 replies
  • 0 kudos

18-bit SPI

Posted on September 25, 2017 at 15:27I'm trying to use two AD7690 (18-bit ADC) http://www.analog.com/media/en/technical-documentation/data-sheets/AD7690.pdf (page 20)But when I accept the data, I get a mistake  HAL_ERRORHowever, I'm getting some dat...