STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DfuseDemo on Ubuntu using Wine

Posted on September 29, 2017 at 12:53Hi ,       I am using DfuseDemo for flashing .dfu on to my stm32l476 based board. This is working fine in the windows 7 environment. But , now to build my code i switched linux ubuntu, so i tried installing the D...

Madhu R by Associate II
  • 1481 Views
  • 2 replies
  • 0 kudos

Problem to download STM32Cube F7 firmware

Posted on January 23, 2017 at 09:37Hello everyone,I am trying to download the F7 firmware package using this link : https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-s...

STM32F777 revision A RMII errata symptoms

Posted on April 29, 2017 at 06:38Ethernet section of my custom board is the same as the STM32F746 discovery board. The same code (start ethernet and reply to ping) works reliably on the discovery board. But on my board (at all speed and duplex modes...

Resolved! Deinitialize USB_OTG_FS

Posted on October 02, 2017 at 11:07Hello!I use cube usb library for usb_otg_fs mode wit STM32L467. I would like to use DM and DP pins also as GPIO INPUT PULL UP when usb is not used.After usb connection closed, I do the following:1) I use functions ...

STM32 USB CDC and Labview

Posted on September 29, 2017 at 15:47Hallo everybody,i have a problem with the communication between a USB CDC Device and the PC Software Labview.On the pictures below you can see my cube settings and labview settings.When i try to open the virtuell...

0690X00000608R4QAI.png 0690X00000608R5QAI.png 0690X00000608R9QAI.png 0690X00000608RJQAY.png
mfrank9 by Associate III
  • 1021 Views
  • 2 replies
  • 0 kudos

Please, explain me RXFD value in OTG_FS_GRXFSIZ?

Posted on October 15, 2014 at 10:50Hello!Sorry for possible mistakes, English - not my native language.The RM0090 contains on page 1269:OTG_FS Receive FIFO size register (OTG_FS_GRXFSIZ)Reset value: 0x0000 0200Bits 15:0 RXFD: RxFIFO depthThis value ...

shumel by Associate
  • 660 Views
  • 1 replies
  • 0 kudos