STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 I2c1 and USART1 (and USART6) conflict

Posted on October 14, 2017 at 19:32I have an STM32F446RE Nucleo board. I am using I2C1 in interrupt (not DMA) mode, to continuously read data from an MPU9250 accelerometer/magnetometer/gyroscope board. I also use the USART1 to read logs with my lapt...

STM32F765BIT MCU ethernet problem.,

Posted on October 09, 2017 at 16:47Hello ., I am working with STM32F765BIT MCU in our custom board. In this I need to make Ethernet interface working with any of protocol (like UDP).I have generated code using STM cube , but I am not sure that I am ...

STM32CubeMX 4.20 BugReport (ADC Dual Mode)

Posted on March 31, 2017 at 03:51I'm using STM32CubeMX 4.20 and STM32CubeF1 v1.4.0 HAL driver. There is a bug when you configure the ADC1 as dual regular simultaneous mode. The code generator adds multi-mode configuration for both ADCs (master and s...

STM32F107 UART Interrupt issue with HAL

Posted on October 10, 2017 at 00:18Hi,I've a question regarding the HAL UART Environment. I could observe that the Interrupt are raised sometimes 2x although  I'm sending only one Byte for the STM32 where I'm reading each single byte.At which condit...