User Activity

Posted on July 05, 2017 at 18:30STM32F7 USB HS host, in FS speed, with external PHY, no VBUS control (always on). The stack fails to detect USB pendrive if it is inserted before reset. I found there is interrupt but seem like the driver does not in ...
Posted on June 15, 2017 at 11:24Hi everybody, I have a custom board with STM32F777 + 800x480 TFT LCD (NHD-5.0-800480TF). The interface is RGB24 bit. LTDC color format is RGB565. Pixel clock is 25MHz.I found that some color seem to be displayed incor...
Posted on April 29, 2017 at 06:38Ethernet section of my custom board is the same as the STM32F746 discovery board. The same code (start ethernet and reply to ping) works reliably on the discovery board. But on my board (at all speed and duplex modes...