STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Seeking A-to-Z for STM32F042 usb to Android

I have a small third-party board with an STM32F042 on it. When I connect it via USB to my Windows 10 computer, it automatically shows up as a COM port. When I connect it to my Ubuntu (VM), it also automatically shows up as /dev/ttyACM0. I also see th...

STM32F051xxx no examples.

Hello, I don't find nothing about this processor, so  Why F051 board and processor doesn't have project/examples?Motor demo board F051 based example/projects again is not in the list. I am using Linux version of tool, FW STM32Cube_FW_F0_V1.9.0

SPI DMA continuous sending

hello...ok so I have managed to get the SPI port on my 446RE nucleo board sending out data to my slave Bus Expander IC via the DMA peripherial.I am new to the DMA peripheral and not sure if I even need to use it over using interrupt control, but woul...

JHERI by Senior
  • 1427 Views
  • 1 replies
  • 0 kudos

Questions related to USB in STM32F429

Is this possible to use internal USB OTG HS PHY in FS mode in STM32F429NI with 1.8V VDD? Internal USB OTG FS PHY needs VDD>2.7V. USB OTG HS in HS mode needs external PHY connected via ULPI. Would OTG HS PHY in FS mode work with VDD = 1.8V?

MLaso by Associate II
  • 3399 Views
  • 9 replies
  • 0 kudos

TCP to Modbus RTU client

Hello allI am new in this forumAnd would like to get yours help regurding adding to my working code the TCP to Modubs RTU client protocol.the code is working on STM32F103 and I intend to add to my PCB Ethernet TCP to Serial RS232 Module in order to e...

IIsha by Associate
  • 1408 Views
  • 2 replies
  • 0 kudos