STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Get serial port buffer size

Posted on December 18, 2017 at 08:14Hi All,   I'm using FreeRTOS and NUCLEO-F746ZG. Is there a way to get the size of the serial port buffer memory? The only way that I found is using register but I'm looking for a better solution.@arg UART_FLAG_RXN...

USB VIRTUAL COMM (WDF_VIOLATION) on the STM32F4

Posted on December 19, 2017 at 19:50I am working with the HAL library with cube as the code generator. I am using the USB virtual comm and it seems it was working fine in the beginning; however, when I am transferring a a lot of data my PC will some...

cleonb322 by Associate III
  • 449 Views
  • 0 replies
  • 0 kudos

[STM32F407] CS43L22 problem!

Posted on December 16, 2017 at 02:40Hello!I am working with CS43L22 on STM32F407VG Discovery Board. I use Audio_playback_and_record example to play .wav file. If i use headphone, I can get good sound. But If I use speaker I get small sound. Is that ...

STM32 Microcontroller USB interface

Posted on December 18, 2017 at 15:17Hello.,I am working with STM32F7 MCU in custom board, Actually it has two onboard MCU(both are STM32F7 microcontroller), Now my first task is to establish USB communication between two MCU's . I tried by configuri...

STM32CubeF0 - SPI functions problem

Posted on July 13, 2016 at 09:27Hi All,We are using STM32F072B and faced with SPI comm. problem.I have seen that Cube SPI functions have some bugs. HAL_SPI_Receive does not reading first three byte and loosing last three byte. I have seen several bu...

0690X00000602xaQAA.jpg 0690X000006036gQAA.jpg

Resolved! SMT32L4 - SD card data transfer to PC

Posted on December 16, 2017 at 14:15Hi,I would like to make a device that works like a memory card reader:I want to share SD card's data in the PC. I would like to connect memory card to discovery board and using USB interface to transfer data.can i...

lorant124 by Associate III
  • 877 Views
  • 1 replies
  • 0 kudos

SPI Callback doesn't work the second time

Posted on December 13, 2017 at 03:32Hi,I'm trying to implement SPI Tx and Rx with LL API. In stripped down code, I have these in my initialization function:LL_SPI_EnableDMAReq_RXLL_SPI_EnableDMAReq_TXLL_DMA_ConfigTransfer(DmaInstanceT, DmaStreamT,LL...

usama2 by Associate II
  • 480 Views
  • 0 replies
  • 0 kudos