STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32h735g ADC3 Support in Zephyr

I am trying to use pins on ADC3 of an STM32h735g in Zephyr, but I am getting a "Could not read (-22)" error, despite not having issues with ADC1. Is ADC3 supported? If so, can you help me with how to configure it?This is based on the Zephyr samples/d...

anthonyog by Associate II
  • 2011 Views
  • 13 replies
  • 2 kudos

Resolved! USB PD AVS support in X-CUBE-TCPP

Hello, I don't seam to see anything related to the implementation of the USB PD AVS system to allow a sink to request voltages of up to 48V. Am I miss-reading the X-CUBE-TCPP code? If it is missing, is there a plan to implement it? Thanks a lotHave a...