STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! I2C-Slave Sample Souce for STM32F303

Everyone, I would like to tell you. I will use the HAL library for the first time. What functions should be called in the main loop for write commands and read commands from I2C-Master? I am very happy if you can provide a sample source. I saw the so...

Kazu by Associate
  • 1319 Views
  • 1 replies
  • 0 kudos

STM32F446ZC FLASH memory organisation

Dear,I use a STM32F446ZC and i don't find the FLASH memory organisation.Neither in the Datasheet orthe ReferenceManual, this organisation is describe.In the ReferenceManual, the memory organisation describe is for the STM32F446ZE with 512kB of FLASH ...

YDann.7 by Associate III
  • 1268 Views
  • 2 replies
  • 0 kudos

stm32l476 CAN functions only in loopback mode

Hi all, I have two stm32l476RG nucleo boards connected via transceivers. Each of them works fine in loopback mode. however none receives messages of the other in CAN_MODE_NORMAL. I'm using a simplistic code ported from STM32L476G-EVAL HAL examples...

mh_stm by Associate II
  • 865 Views
  • 0 replies
  • 0 kudos

STM32F407 USB CDC data transmission

Hello all,I am using STM32F407 , in that i am able to communicate with USB Full speed mode. In that i am trying to send data serially from android phone which act as a Host and STM32F407 act as Device. When i trying to send 2KB data serially to my US...

USB_CDC on STM32F0 series

I'm trying USB_CDC FS (Full Speed) on STM32F072C8 Controller. I'm able to Transmit data larger than 64 bytes to PC, but not able to receive data more than 64 bytes.I'm using CDC_Receive_FS function for receiving and buffer size is 1000.If i send 100 ...

BPR by Associate II
  • 2422 Views
  • 6 replies
  • 0 kudos