cancel
Showing results for 
Search instead for 
Did you mean: 

I2C-Slave Sample Souce for STM32F303

Kazu
Associate

Everyone, I would like to tell you. I will use the HAL library for the first time. What functions should be called in the main loop for write commands and read commands from I2C-Master? I am very happy if you can provide a sample source. I saw the source file made with STM32CubeMX, but I did not understand.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

There are example projects inside the Cube package:

STM32Cube_FW_F3_V1.10.0/Projects/STM32F303K8-Nucleo/Examples/I2C

View solution in original post

1 REPLY 1

There are example projects inside the Cube package:

STM32Cube_FW_F3_V1.10.0/Projects/STM32F303K8-Nucleo/Examples/I2C