2019-02-27 2:29 AM
Hi all,
I have two stm32l476RG nucleo boards connected via transceivers. Each of them works fine in loopback mode. however none receives messages of the other in CAN_MODE_NORMAL.
I'm using a simplistic code ported from STM32L476G-EVAL HAL examples. Both boards have same configuration: clock 16MHz for all buses, same pins,... all CAN IDs are accepted. Both MCUs have CAN1_RX0_IRQn enabled but never triggered.
Here is the configuration:
/*
* @name com_gpio_config.
* @brief sets up CAN GPIO pins.
* @param none.
* @retval none.
*/
static void
com_gpio_config (void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* Enable GPIO clock */
__HAL_RCC_GPIOA_CLK_ENABLE ();
/* Configure peripheral GPIO */
GPIO_InitStruct.Pin = GPIO_PIN_11 | GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Alternate = GPIO_AF9_CAN1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
return;
}
/*
* @name com_can_config.
* @brief configures CAN peripheral.
* @param none
* @retval none
*/
static void
com_can_config (void)
{
CAN_FilterTypeDef sFilterConfig;
/* peripheral clock enable */
__HAL_RCC_CAN1_CLK_ENABLE();
/* configure the CAN peripheral */
can_handle.Instance = CAN1;
can_handle.Init.TimeTriggeredMode = DISABLE;
can_handle.Init.AutoBusOff = DISABLE;
can_handle.Init.AutoWakeUp = DISABLE;
can_handle.Init.AutoRetransmission = ENABLE;
can_handle.Init.ReceiveFifoLocked = DISABLE;
can_handle.Init.TransmitFifoPriority = DISABLE;
can_handle.Init.Mode = CAN_MODE_NORMAL;//CAN_MODE_LOOPBACK;//
can_handle.Init.SyncJumpWidth = CAN_SJW_1TQ;
can_handle.Init.TimeSeg1 = CAN_BS1_16TQ;
can_handle.Init.TimeSeg2 = CAN_BS2_2TQ;
can_handle.Init.Prescaler = 32;
if (HAL_CAN_Init(&can_handle) != HAL_OK)
{
/* halt process */
while (1);
}
/* configure the CAN Filter */
sFilterConfig.FilterBank = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = CAN_RX_FIFO0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.SlaveStartFilterBank = 0; // unique CAN instance
if (HAL_CAN_ConfigFilter(&can_handle, &sFilterConfig) != HAL_OK)
{
/* halt process */
while (1);
}
/* start the CAN peripheral */
if (HAL_CAN_Start(&can_handle) != HAL_OK)
{
/* halt process */
while (1);
}
/* activate CAN Rx IRQ */
if (HAL_CAN_ActivateNotification(&can_handle, CAN_IT_RX_FIFO0_MSG_PENDING | CAN_IT_RX_FIFO0_FULL) != HAL_OK)
{
/* halt process */
while (1);
}
/* configure transmission process */
tx_header.StdId = 0x321;
tx_header.ExtId = 0x01;
tx_header.RTR = CAN_RTR_DATA;
tx_header.IDE = CAN_ID_STD;
tx_header.DLC = 2;
tx_header.TransmitGlobalTime = DISABLE;
HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 2, 0);
HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
return;
}and here is the sending loop:
if (HAL_CAN_AddTxMessage(&can_handle, &tx_header, (uint8_t*)&msg, &tx_mailbox) != HAL_OK)
{
/* Transmission request Error */
cli_error ("CAN Tx failed");
retval =(-1);
}
else
{
cli_notice ("command sent!");
}
simple _delay (some_time);