cancel
Showing results for 
Search instead for 
Did you mean: 

Bug HAL_delay() off by 1ms

Lama
Associate III

By coincidence I discovered a bug in HAL_delay().

__weak void HAL_Delay(uint32_t Delay)

{

 uint32_t tickstart = HAL_GetTick();

 uint32_t wait = Delay;

 /* Add a period to guaranty minimum wait */

 if (wait < HAL_MAX_DELAY)

 {

   wait++;

 }

 while((HAL_GetTick() - tickstart) < wait)

 {

 }

}

Since HAL_MAX_DELAY is 0xFFFFFFFFU you always get a 1 ms bonus. Please fix it ST this is pretty sloppy. I wonder how you test your software.

This is for MCU package STM32Cube_FW_L4_V1.13.0.

This discussion is locked. Please start a new topic to ask your question.
9 REPLIES 9
waclawek.jan
Super User

> you always get a 1 ms bonus

No, you don't. It depends on where within the granularity of HAL_GetTick() you call this function - it may well be that it's just about to tick when tickstart is read, and then the delay lasts almost exactly the length you requested. In other words, this ensures that the delay is *at least* of the requested length.

JW

Realistically if want better precision you start with a finer granularity time base, just saying...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Lama
Associate III

Ok, understood, the semantic of the call is that you wait for at least the number of milliseconds specified. The granularity of the timer is 1ms.

So without the bias at an arbitrary moment the expected delay for n>0 would be: (n-0.5)±0.5ms with the bias (n+0.5)±0.5ms

However if two HAL_delay() calls are called directly after each other the second one will have a bias of 1ms.

Without the addition the minimum wait of the routine could be approaching zero.

One would really use a TIM clocking at 1 MHz and NOT interrupting, or DWT_CYCCNT to get some meaningful precision in timing..

HAL_Delay() is a blunt axe and used as such. Better than the initial attempts which didn't handle wrapping properly.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Lama
Associate III

@Community member​  Indeed, I was using a HiRes timer, to test it I profiled HAL_Delay() and observed it's behavior that was well explained by @Community member​ 

Zek_De
Senior

what about if Delay is close overflow value, in this case code have to wait a lot to reach value expected

It is coded correctly to work across the 32-bit wrapping point, the code originally did not, and that's been beaten into a few people now.

start = current;

while((current - start) < delay);

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I couldnt understand well.

for example let's assume about uint8_t and delay = 100 ms

uint8_t start = current(also assume this is uint8_t)

assume start = 250

while((250 - 250) < 100)

while((251 - 250) < 100) like that and number will get overflow and I have to wait more and more to catch < 100 ms

oh sorry , my fault .I handled it.