STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want ST offer a interface HAL_UART_DMAStop_RX

I use stm32cubemx. And in stm32fxxx_hal_uart.c. There is a function "HAL_UART_DMAStop". This function will stop both TXDMA and RXDMA.But I have a request. I often use "HAL_UART_DMAStop"+"HAL_UART_Receive_DMA" to flush dma buffer. But HAL_UART_DMAStop...

STM Virtual Comm Port (VCP) driver slow on Windows 7

I have an STM32F4 device that uses the USB peripheral and CDC driver.I have a portable python app that communicates with the STM32F4 from Mac OS X 10.13 (High Sierra), Win10 and Win7.On Mac and Win10 the app communicates with good speed, however on W...

BSimo by Associate
  • 556 Views
  • 0 replies
  • 0 kudos

Bug on SDcard and stm32f415 ?

Hi, i have a problem with my project....I'm using Fat and SD with freertos to read/write files on SD using hdma channel.First part i fixed all "SDIO_STA_STBITER" with "SDIO_STA_STBITERR" (with 2 "R" ) because a typo is present.But i see the interrupt...

Marco1 by Associate II
  • 2153 Views
  • 9 replies
  • 0 kudos

['F407 OTG] Is OTGx_HPRT.PENA rc_w0?

In RM0090 rev.17 both OTG_FS and OTG_HS, the HPRT.PENA is described as rc_w0.However, the code in Cube does not support this; rather, it seems it's rc_w1.RM0390 says it's rc_w1, and although it's a slightly different revision of the OTG core, I'd say...

STM32F072B-Discovery TSC Cube Project

I try to generate TSC project by using STM Cube,but I am not sure how to write this function: void HAL_TSC_ConvCpltCallback(TSC_HandleTypeDef* htsc).There is same function in "STM32Cube\Repository\STM32Cube_FW_F0_V1.9.0\Projects\STM32F072B-Discovery\...

STM32L152 Bootloader Extended Erase Failure

Using our internally developed tool for writing a binary to a target using the in-ROM Bootloader according to AN3155 and AN2606, we were unable to appropriately perform commands as described in both application notes, specifically Bootloader Extended...

CVoro by Associate II
  • 903 Views
  • 2 replies
  • 0 kudos