STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

addin HAL driver to blinky project

I have started from blinky project and want to extend it for some PWM outputs on TIM2.For this I need to make use of stm32f3xx_ll_tim.h.I added into my main.c #include <stm32f3xx_ll_tim.h> without successI added the file from 'Manage project Items' a...

SKaro by Associate II
  • 4117 Views
  • 10 replies
  • 0 kudos

USB HID composite for multiple device

Hi there,ENV: I use a Nucleo-L412KB board with ST library, STM32Cube_FW_L4_V1.13.0. PURPOSE: I am trying to connect my board to pc via USB and send mouse, keyboard and multi-touch reports to PC. In this project, I want my PC to read my board as USB c...

XYan.6 by Associate
  • 993 Views
  • 0 replies
  • 0 kudos

Audio example using STM32F769 Discovery board

What is a relatively easy/simple way to process analogue audio from the jacks on the STM32F769 Discovery board ? Is there already a template for this ?I would be very grateful for any assistance with this.I am new to programming DSP hardware, althoug...

MLawr by Associate III
  • 2517 Views
  • 4 replies
  • 0 kudos

I2C Slave Transmit Problems

I want to use a STM32L151RDT6 as I2C slave and a USB to I2C bridge from FTDI as master.Reading command with the slave from the master is possible. But when i try to transmit data to the master the slave is releasing the SDA Line after the acknowledge...

0690X000008wBHoQAM.bmp
JM?�l by Associate II
  • 1100 Views
  • 0 replies
  • 0 kudos

Problem with 8MHz clock and bootloader for USB

Hello, I have this design but I think the clock does not rock me. How can I check it without having an oscilloscope? I have a voltmeter but I measure the voltage at both ends and it varies only between -100mV and 100mV ...I have made a bootloader to ...

FFran by Associate II
  • 640 Views
  • 0 replies
  • 0 kudos

STM32F07 - IAP question, jumping from base 0x08000000 to Application offset. Interrupts not working.

Hi,​I’ve sectioned the STM32G071 into 2 sections with the IAP portion booting up as per default 0x0800000. I’ve also downloaded @ 0x0800A000 the main application code that I would like to run.​During boot, the IAP code executes first and it runs fine...

Dng.14 by Associate
  • 895 Views
  • 0 replies
  • 0 kudos