STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with STM32F746G-DISCO board

Hi I have just purchased the STM32F746G-DISCO board and just powered up to test the demo software. Touchscreen looks really good, but after I plugged in my ethernet cable it comes up with "cable not connected" even though it is (with the orange led ...

USB CDC - Maximum Baud Rate of device side (not host)

I am working on STM32L496 nucleo board. I would like to transfer data from STM32L496 (as device) to host PC (RX is not required).currently, the baud rate is ~200kbyte. no matter if I am increasing the packet size (CDC_DATA_FS_MAX_PACKET_SIZE) to 512...

AA.10 by Associate III
  • 1721 Views
  • 1 replies
  • 0 kudos

Reserved bits of registers.

Hello, I have a question related to the reserved bits (generally to all of them). For example lets disscus specification of STM32F429 MCU from the RM0090:Register TIMx_SR1 (of TIM2 to TIM5 for example) has specified bits 5, 7, 8, 13, 14, 15 as reserv...

Software Timer API problem+freertos

/* Create the timer(s) */ /* definition and creation of myTimer01 */ osTimerDef(myTimer01, Callback01); myTimer01Handle = osTimerCreate(osTimer(myTimer01), osTimerPeriodic, (void*) 1); /* USER CODE BEGIN RTOS_TIMERS */ /* start timers, add new ones, ...

km naxin by Associate II
  • 777 Views
  • 0 replies
  • 0 kudos

STM32H7x3.svd is incorrect

Debugger information is displayed incorrectly because STM32H7x3.svd (and others!) in latest version V1.4 seem to be wrong regarding register address offsets of DFSDM module (and maybe others?). At least addresses do not match the latest spec ("RM0433...

MMein by Associate
  • 1140 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.