STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F030 Bootloader Go

I have the following situation. I use a STM32F030F4 flashed with a programm created with Keil uVision. I use startupfile provided from ST. Flashtool and Target dialog are configured in "default". The address for the app inside the flash starts at 0x0...

0690X000008iKqSQAU.jpg
klaus2 by Associate II
  • 3025 Views
  • 5 replies
  • 0 kudos

Problem using audio on STM32F7

Hi!I've been struggling for several days in trying to make a working audio example on my STM32F746 Discovery board.I have studied the datasheet of the codec, of SAI, I2S and the examples given in the STM32F7 firmware package.I have succeeded in makin...

SPI bandwith using HAL ?

I'm testing the SPI capabilities of STM32H7. For this I'm using the SPI examples provided in STM32CubeH7. I will perhaps not keep this code in my own development, rigth now the goal is to understand how SPI is working and what bandwith I can get in t...

Gpeti by Senior II
  • 2514 Views
  • 7 replies
  • 0 kudos

Resolved! I maked simple program with LWiP, and call netconn_bind(conn, IP4_ADDR_ANY, port) halted MCU board nucleo-f767zi.

I maked simple program with LWiP. After I got dinamyc address, I tried socket connection and call netconn_bind halted MCU.My code: for(;;) {  if(OK_D == 0)    {    IP_A = gnetif.ip_addr.addr;    if(IP_A == 0)    {      HAL_GPIO_WritePin(GPIOB, GPIO_P...

0690X000008wQQqQAM.png

usb disk error problem in stm32f105rb?

hi Im using stm32f105rb mcu to read files from usb using fatfs libraries and i am able to read upto 17 files simultaneously more than that will shoot a disk error. what will be the root cause and is it possible to read more then 50 files simultaneous...

sprak.2 by Associate
  • 1795 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.