SPI bandwith using HAL ?
I'm testing the SPI capabilities of STM32H7. For this I'm using the SPI examples provided in STM32CubeH7. I will perhaps not keep this code in my own development, rigth now the goal is to understand how SPI is working and what bandwith I can get in the different modes (with DMA, with cache enabled or not, etc...).
I'd like to share the figures I've computed, as it doesn't seem very high. In the example, if I understood correctly, the CPU is @ 400Mhz and the SPI bus frequency @ 100MHz.
For polling mode I've measured the number of cycles of the call to function HAL_SPI_TransmitReceive.
For DMA I've measured between call to HAL_SPI_TransmitReceive_DMA and call to the transfer complete callback.
Measurements of cycles where made with SysTick clocked on internal clock. Since there is no low power usage, it should be accurate.
I've just modified ST's examples to send a buffer of 1KB.
I get around 200.000 CPU cycles in polling mode, which means around 2MB/s
And around 3MB/s in DMA mode.
Since the SPI clock runs at 100Mhz I would have expected much more, especially in DMA mode, what do you think ? Is there something wrong in my test procedure ?