STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F303VB: How to debug Boot loader + Application?

Posted on August 04, 2017 at 08:19Hi,I'm working on my custom hardware based on STM32F303VBI'm trying to make a CAN based boot loader. I can jump from boot loader to application but the application just hangs some where.How can I debug boot loader +...

Prasant J by Associate III
  • 2647 Views
  • 7 replies
  • 0 kudos

I am developing custom board with STM32F207 as slave Micro Controller . The Master Controller will Fork the STM32F207 and transfer application firmware over SPI . I need complete source code for SPI Boot loader STM32F207 .

I am developing custom board with STM32F207 as slave Micro Controller . The Master Controller will Fork the STM32F207 and transfer application firmware over SPI .I need complete source code for SPI Boot loader STM32F207 .

USBDevice/CDC Standalone Example not working USB FS

Hi,i tried to use the USB Device CDC Standalone example to make my MCU (STM32F407iG) working as a USB TO Serial Converter Bridge like a PL2303TA Chip. But somehow the USB FS doesn't connect to my PC. What am i doing wrong do i need to change the cloc...

arduo by Senior
  • 597 Views
  • 2 replies
  • 0 kudos

why ethenet is not working on stm32f769i?

HI, I just bought STMF769i-eval and started with lwip examples from the FW . but there are not working, even i can't ping. then I read about Solder brigdes and de solder some of the brigdes and try again but still unable to ping. is that hardware pro...

embo by Associate II
  • 455 Views
  • 0 replies
  • 0 kudos

STM32 usb bus powered limitation

We are currently developing a portable device with a STM32F4 display and so on. It is usually powered with non-rechargeable batteries (4x AA LR6). It consumes at least 140mA and max 450mA. As everyone has a micro usb cable and power plug, we thought ...

JB91 by Associate II
  • 650 Views
  • 1 replies
  • 0 kudos

Programming BRR Register

Hi,how can i program the BRR Register in the USB Device CDC Standalone example for STM32F4xx?The Example code uses  UartHandle.Init.BaudRate   = 9600;How can i directly access to USART_BRR Register?

arduo by Senior
  • 609 Views
  • 1 replies
  • 0 kudos