STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Composite Device COM PORT

Hi there,i managed the get a working composite device with working driver files. I can choose between all combinations of cdc,hid and msc.But i can't connect to my serial com port. I want to use this com port as a uart bridge but it's not working bec...

arduo by Senior
  • 444 Views
  • 0 replies
  • 1 kudos

Problem with SDMMC1 and 4bit Wide Bus

Hello,I have a STM32H743ZI with FreeRTOS and SDMMC1 initialized from MxCube 5.0.1.I'm currently using the FreeRTOS-FAT.When i try to call a HAL_SD_WriteBlocks_DMA() with 4bit wide bus, I always get "HAL_SD_ERROR_DATA_TIMEOUT" in the IRQ Handler. With...

Is an MP3 encoder available for the STM32F733

The CubeMX samples have an MP3 encoder, but it appears to be a binary blob rather than source, and locked to certain chips & versions of the libraries. Is it possible to get the source or is a compiled version available for the STM32F733 / STM32F723?

AGoel.5 by Associate
  • 513 Views
  • 0 replies
  • 0 kudos

Using HAL outside of main.c

Ok, another noob question....I can use the following line of code in the main.c with no issues#define Green_LED_OFF HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET); // Green offBut when I want to use it in another .c file such as foo.c I get th...